Part Number: DS90UB914A-Q1
Hi Team,
I was wondering with the 914 if there is any way to shift 8-bit raw data to the upper or lower 10-bit output (similar to how the 954 can do this with Reg 0x7C - PORT_CONFIG:RAW10_8BIT_CTRL
Thanks!
David
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB914A-Q1
Hi Team,
I was wondering with the 914 if there is any way to shift 8-bit raw data to the upper or lower 10-bit output (similar to how the 954 can do this with Reg 0x7C - PORT_CONFIG:RAW10_8BIT_CTRL
Thanks!
David
Hi Shumate,
Unfortunately, UB914a is NOT like UB954 with CSI2 frame generation, it is one PHY de-ser, and the parallel output pins are matched with UB913a/933's parallel input pin accurately.so you can't shift/re-order the parallel output signals.
best regards,
Steven