Part Number: TPS25810
Other Parts Discussed in Thread: TPS2547,
Team,
I have a dual USB charging application with one USB-C and one USB-A port. For this TPS25810 and TPS2547 should be used. Current limitation needs to be as this:
- If only on USB-C a device is connect, current should be limited to 3 A
- If only on USB-A a device is connect, current should be limited to 3 A
- If both ports are connected, limit on USB-C should be 1.5 A and on USB-A 0.9 A
How can this be achieved with ILIM_SET and /LD_DET pins of both devices?
Thanks,
Robert