Part Number: TUSB321
Does this IC include the Rp pullup resistors for CC1 and CC2 pins or should they be added to my PCB?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB321
Does this IC include the Rp pullup resistors for CC1 and CC2 pins or should they be added to my PCB?
Hi Malik- Thanks. Follow-up question though. In the Universal Serial Bus Type-c Cable and Connector Specification Rev 1.3, section 4.11.1 Termination Parameters, Table 4-20 gives basically 6 different CC pullup R values depending on the combination of advertised source current and the pull-up voltage. Are you saying that the IC is designed to present the "correct" Rp based on what these two values are?
tnx
Chuck
Hi Chuck,
My apologies let me clarify my previous post. TUSB321 has a internal Rp current source that is used to report specific states on the CC line. For reference, you can see this illustrated in the functional block diagram in section 7.2 Functional Block Diagram. The correct current is sourced onto the CC line based on TUSB321 settings. Also there are only three Rp resistances based on the given internal pull-up voltage, this value is typically separate from Vcc.