This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM recommendations



Hello:

I am looking for an ANALOG 5-wire RGB to serial 5-pair LVDS video and a ARM Processor to output serial 5-pair LVDS video evaluation boards with open source schematics for the following two applications below.

1.         Evaluation board with open source schematics to convert ANALOG 5-wire RGB (R + G + B + HS + VS) 640 x 480 60p video to LVDS 5-pair D0+, D0-, D1+, D1-, D2+, D2-, D3+, D3-, CLK+, CLK-, video output to drive a LVDS LCD display. I will also buy a LVDS LCD display from you if it’s a direct connection to the evaluation board. Once all is working my plan is to layout my own PCB. All components must have a temperature range of at least -40 °C to +85 °C,

2.         Evaluation board with open source schematics for a ARM Processor to ingest 10/100 Ethernet and then have a LVDS 5-pair D0+, D0-, D1+, D1-, D2+, D2-, D3+, D3-, CLK+, CLK-, video output to drive a LVDS LCD display. My plan is to host the QT software under Linux on the ARM processor to extract data from the Ethernet packets to drive the LVDS LCD display. If the ARM processor only has a 24-bit color parallel digital RGB output then provide a second evaluation board to convert that to LVDS 5-pair D0+, D0-, D1+, D1-, D2+, D2-, D3+, D3-, CLK+, CLK-, video. I will also buy a LVDS LCD display from you if it’s a direct connection to the evaluation board. Once all is working my plan is to layout my own PCB. All components must have a temperature range of at least -40 °C to +85 °C,

Thank-you

Mark Long

NAWCAD

mark.long@navy.mil

 

 

  • Mark,

    I am not aware of a single device from TI that performs this interface conversion.  Our new AM654x devices contain an OpenLDI video output that is similar to what you describe and it can be operated in a raw LVDS mode.  It also supports serial video in using a CSI2 interface.  If you can find video converter devices to adapt to the existing interfaces, then this device will meet your needs.

    Tom

    http://www.ti.com/product/AM6548