This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25810: Schematic Review

Part Number: TPS25810

Team,

Please help to review the attached schematic.

USB-Schematic.pdf

The requirements are as below:

Simple USB-C port with USB 2.0 support

1) CC Pin Port Controller (with Pullups/down - no PD communication)

              (A) DFP (Downstream Facing Port) only

              (B) USB 2.0 Power Mode (max 500mA @ 5V)

2) Current limiter (Turn-off / current limit @ 500mA)

3) Overcurrent Flag/Pin

4) Enable Pin

5) ESD Protection (15kV Air/ 8 kV Cond.)

Regards,

Sanjay R. Pithadia