Part Number: DS90UB954-Q1
Hi team,
I have some questions.
#1.
What is the state of the CSI output when Lock is unintentionally dropped during normal operation?
Does the 954 try to keep sending data with errors, or is it in the LP11 state?
#2
Does the ser keep trying to send the received MIPI CSI data to 954 even if the lock is lost?
#3
If Port 0 Receiver Enable is set to "0-> 1" while receiving HS from the Ser side, will DPHY-Cp / Cn output LP-11?
I think LPS output will not be output during the image blanking period, because the clock is in “Continues” mode.
Is LPS status output only when Port 0 Receiver is enabled from disabled?
Best regards,
Tomoaki Yoshida