Part Number: DS90UA101-Q1
Other Parts Discussed in Thread: DS90UA102-Q1
I have SerDes link design using DS90UA101-Q1 and DS90UA102-Q1. I need to have a serializer clock of 32.768MHz, which equates to line rate of 917.504MHz.
The application requires use of CAT-type cabling. However, I cannot use CAT7 due to system requirements, CAT6 as maximum. The maximum cable length is only 10m, not the full 100m spec of CAT6. Will CAT6 cabling support a 917.504MHz line rate, if the cabling distance is limited to 10m?
Thanks!