Part Number: TPS65981
Our device uses the TPS65981 as a PD controller. It is a UFP, but it is capable of doing a power role swap in order to charge the connected host device. This is all working fine when the connected device is powered on. The BARREL_JACK_DET gpio is triggered and the role swap succeeds. However, if the connected device is turned off, triggering the BARREL_JACK_DET input has no effect. When a charger is connected to a device that is off, I believe it begins by providing standard 5V to the device, and can then negotiate to other power levels. Is there a way to get the TPS65981 to provide this initial power to a device that is off in order to function as a charger?