This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HD3SS3220: Start up with ENN_CC = Low

Part Number: HD3SS3220


Hello team,

Customer is thinking to avoid generating interrupt by CC detection at start up.

For that, they want to start up the device with ENN_CC=High(Disable). And then, once the processor is ready, they will set ENN_CC to Low(Enable).

When above control is used, is ADDR pin needed to left OPEN?

Otherwise, even if ADDR pin is Low/High (I2C mode), is it available to enable and disable control of CC detection by CC_ENN pin?

Regards,

Saito