This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822IF: Link is still established in low BER condition

Part Number: DP83822IF


Hello,

I saw AFBR-5803 used in reference design. Please let me ask if DP83822IF keep link established when  AFBR-5803 used for fiber module.

In AFBR-5803 datasheet, deassert level is written below. It will be BER rate may become 10e-2. Does DP83822IF keep link in this low BER condtion?

DP83822IF becomes not re-established if SD doesn't connect LED_1 except for software reset. We worry DP83822IF can't establish link again If SD is assert but link is broken situation occurs.

Do we think ok this situation doesn't occur in low BER condition?

"The maximum value will occur when the input optical power is either –45 dBm average or when the input optical power yields a BER of 10–2 or larger, whichever power is higher."

Best regards,

Toshihiro Watanabe