This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75DP159: HDMI no display

Part Number: SN75DP159

Hello expert,

My customer got a FA case and the issue is their NB cannot show the screen to HDMI display. After A-B-A testing, we know that issue does follow IC. And impedance is shown as below table. It seems like there are OUT and VDD impedance different. May I know if this IC is still good or can we send to FA step? Thanks a lot!

top side marking 75DP159 75DP159
TI 74I TI 88I
CHFJ G4 A4YD G4
  good sample
impedance
FA sample
impedance
(PIN NO.)  
1 SWAP/POL 70k 68k
2 IN_D2p 68k 67k
3 IN_D2n 68k 67k
4 HPD_SRC 47k 47k
5 IN_D1p 68k 67k
6 IN_D1n 68k 67k
7 GND 0.7ohm 0.8ohm
8 IN_D0p 68k 67k
9 IN_D0n 68k 67k
10 I2C_EN/PIN 90k 90k
11 IN_CLKp 68k 67k
12 IN_CLKn 68k 67k
13 VCC 31k 31k
14 VDD 1.49k 2.2k
15 SCL_CTL 727k 731k
16 SDA_CTL 730k 725k
17 NC 90k 90k
18 CEC_EN 47k 46k
19 GND 0.3ohm 0.7ohm
20 PRE_SEL 70k 67k
21 EQ_SEL/A0 70k 68k
22 Vsadj 25k 24k
23 VDD 2.6k 2.7k
24 VDD 2.2k OL
25 OUT_CLKn 75k 74k
26 OUT_CLKp 75k 74k
27 #HDMI_SEL/A1 90k 90k
28 OUT_D0n 75k 74k
29 OUT_D0p 75k 74k
30 GND 0.3ohm 0.7ohm
31 OUT_D1n 75k 78k
32 OUT_D1p 75k 78k
33 HPD_SNK 191k 185k
34 OUT_D2n 75k 48k
35 OUT_D2p 75k 48k
36 TX_TERM_CTTL 70k 68k
37 VDD 2.2k 2.4k
38 SCL_SNK 751k 760k
39 SDA_SNK 741k 753k
40 SLEW_CTL 68k 67.5k
41 GND 0.3ohm 0.7ohm
42 OE 95k 94k
43 VCC 31k 31k
44 AUX_SRCn 15k 15k
45 AUX_SRCp 16k 15k
46 SCL_SRC 768k 753k
47 SDA_SRC 747k 735k
48 VDD 1.49k 2.2k
Thermal Pad   0.3ohm 0.3ohm

Best regards,

Ann Lien