Part Number: LMH1218
Hello community,
In the LMH1218 data sheet, the 2 level inputs logical levels (VIHmin, VILmax) are not specified.
These levels are only specified for the 4 level inputs and the 3.3V tolerant pins.
Daniel
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMH1218
Hello community,
In the LMH1218 data sheet, the 2 level inputs logical levels (VIHmin, VILmax) are not specified.
These levels are only specified for the 4 level inputs and the 3.3V tolerant pins.
Daniel
Hi Daniel,
This is not clear in the data sheet but it is noted as part of the 3.3-V tolerant LVCMOS/LVTTL section of the data sheet.
In summary, minimum input high voltage is 0.7*VDD(2.5V) or 1.75V and maximum input low voltage is 0.8V(~0.3*VDD).
Regards,, Nasser