Part Number: TIC12400-Q1
Hi,
I am using TIC12400-Q1 for multiple switch detection in one of my project. I have following requirement
- While ECU is in awake state polling should be 8ms
- While ECU is in Sleep state polling should be 48ms
While entering into sleep state, I've to clear CONFIG Register (Offset = 1Ah) by SPI_CMD(0xB4000001) and then I make new polling configuration.
Here my observation, whenever I make TRIGGER(Bit11) to 0, interrupt is generated on INT pin. My INT pin is working as an WAKE-Up signal to ECU. Due to which I am not able to enter into sleep state.
Could you please suggest me, how should I suppress this interrupt generation while switching to new polling configuration??
Thanks in Advance!!