Part Number: TCAN1043-Q1
Hi Team,
Customer is asking if TCAN1043-Q1 support ISO 16845. Please help to double confirm. Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN1043-Q1
Hi Team,
Customer is asking if TCAN1043-Q1 support ISO 16845. Please help to double confirm. Thanks
Helios,
The ISO 16845 standard is a conformance test plan based on the specifications of ISO 11898-1 (CAN data link layer definition), and then was later updated to include static and dynamic tests for compliance with ISO 11898-2:2016 as well (CAN high-speed medium access unit definition). This document is referenced in C&S testing (CAN conformance certification) reports, and the TCAN1043-Q1 went through this certification prior to release. If the customer would like to see the report, please email me directly and I can share the document with you.
Please let me know if you have any other questions or concerns.
Regards,