This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822I: equalizer function, compliance test, and distance

Part Number: DP83822I

Hello Team,

I would like to confirm 3 things about DP83822IRHBR

(1) Equalizer function

Is its function analog method or digital method ?

(2) Compliance test

Did we confirm that DP83822 has passed the ethernet compliance test on our EVM (or other condition) ?

(3) Cable distance

Can DP83822 meet the transmission distance: 20cm or less & 110m or more ?

Any advice will be appreciated.

Jin

  • Hello Jin,

    1) "The DP83822 uses mixed-signal processing to perform equalization, data recovery, and error correction to achieve robust operation over CAT5 twisted-pair cable."

    2) Yes

    3) All cable length under 150 m.

    Thanks,

    Vibhu

  • Hello Vibhu,

    Thanks for your help.

    About (3), My customer still concerns about short length condition....Less than 20cm.

    Can we say DP83822 could appropriately work in the range ?

    Best Regards,

    Jin

  • Hello Vibhu,

    I have one more question about DP83822.

    Let me summarize as below

    (1) In short cable length condition (less than 20cm)

    Can we say DP83822 could appropriately work in the range ?

    I remember EtherNET PHY compliance test uses shorter cable than 20cm. So it should be OK, But I hope to have your expertise.

    (2) Clock source for DP83822

    As usage, customer will send a clock signal from MPU to 20Pin (MDC). In that case, CMOS level oscillator source could be acceptable without external crystal ?

    XI pin needs to be connected to Clock signal, Can they connect XI pin with 20Pin (MDC) & XO pin is left floating ?

    *Referring to the data sheet, (RESET timing diagram), MDC & XI clock cannot be same source.....

    In the case of using external crystal for XI, XO pins.

    Can we recommend attached crystal ?

    DX321G-datasheet.pdf

    Any advice will be appreciated.

    Jin

  • Hi Ikeda-san,

    1. Yes DP83822 shall link up and data transfer at short cable lengths of 20 cm.

    2. XTAL recomended specifications are defined in datasheet Applications section. The crystal part you shared has good ppm of 50 and shall be suitable to use.

    Regards,

    Geet