Part Number: DP83TC811S-Q1
Dear all
I had find a question, I use one DP83TC811S-Q1 device as master, use other one DP83TC811S-Q1 device as slave,:
1. When I power up the slave device, then power up the master device, the slave device can not work normally.
2. When I power up the master device, then power up the slave device, the slave device can work normally.
Why ? What's wrong ?
Below is configuration information:
Master:
echo 0xd 0x1 > /sys/class/net/eth0/device/phy_regnum
echo 0xe 0x0834 > /sys/class/net/eth0/device/phy_regnum
echo 0xd 0x4001 > /sys/class/net/eth0/device/phy_regnum
echo 0xe 0xc000> /sys/class/net/eth0/device/phy_regnum
Slaver:
echo 0xd 0x1 > /sys/class/net/eth0/device/phy_regnum
echo 0xe 0x0834 > /sys/class/net/eth0/device/phy_regnum
echo 0xd 0x4001 > /sys/class/net/eth0/device/phy_regnum
echo 0xe 0x8000> /sys/class/net/eth0/device/phy_regnum