Part Number: DS90UB941AS-Q1
Other Parts Discussed in Thread: DS90UB948-Q1
It seems like I can not get the DSI input to the serializer to work properly.
Reported errors:
- DSI Port 0 indirect register 28 - DSI CRC Checksum error - Constantly active
- DSI Port 0 indirect register 0 - Error counter is constantly 0 (Why, if we constantly have errors?)
- Register 5A bit 2 = 0. DSI PLL Not locked. (Should be locked?)
- DSI Port 0 indirect register 3A/3B - Indicates M/N = 2/3, should be 1/3?
Maybe there is something more I have missed
Serializer setup:
Single mode (Single DSI input, single output)
Continuous DSI clock as Bridge clocking mode.
DSI input:
1920 x 720 pixels, 24-bit RGB
Pixel clocks of 95, 91 and 66 MHz has been tested - no difference.
Register readouts are from 66 MHz test.
4 - lane DSI.
Sync signals.
Receiver end is a DS90UB948-Q1 deserializer.
Complete register readout:
Serializer main registers
00: 24 00 00 9A 10 00 58 00
08: 00 01 41 0A 47 30 00 00
10: 00 00 00 BB 00 00 FE 1E
18: 7F 7F 01 00 00 00 01 00
20: 0B 00 25 00 00 00 00 00
28: 01 20 20 A0 00 00 A5 5A
30: 00 09 00 05 0C 00 00 00
38: 00 00 00 00 00 00 81 02
40: 09 3F 00 00 00 00 00 00
48: 00 00 00 00 00 00 00 8C
50: 16 00 00 00 00 00 00 02
58: 00 00 D9 81 07 06 44 42
60: 22 02 00 00 10 00 00 00
68: 00 00 00 00 00 00 20 00
70: 00 00 00 00 00 00 00 00
78: 00 00 00 00 00 00 7E 00
DSI Port 0 indirect registers
00: 00 00 00 18 1C 10 00 00
08: 00 00 00 00 00 00 00 1F
10: 00 00 00 00 00 00 00 00
18: 00 00 00 00 00 00 00 00
20: 7F 60 FF 7F 00 00 00 00
28: 01 FF 3E 04 00 00 00 00
30: 00 20 00 04 00 20 00 00
38: 00 00 02 03 00 00 00 00
DSI Port 1 indirect registers
00: 00 00 00 18 1C 10 00 00
08: 00 00 00 00 00 00 00 10
10: 00 00 00 00 00 00 00 00
18: 00 00 00 00 00 00 00 00
20: 7F 60 FF 7F 00 00 00 00
28: 00 00 00 00 00 00 00 00
30: 00 20 00 04 00 20 00 00
38: 00 00 02 03 00 00 00 00
I have tried to change DSI timing parameters.
This can make DPHY errors appear, but does not seem to get anything else better.
Anya ideas?
/Peter