Part Number: DS250DF230
Other Parts Discussed in Thread: , SIGCONARCHITECT
Hi Team,
My customer considers to use DS250DF230 under the following data rates.
・25.78125 Gbps
・10.3125 Gbps
・9.8304 Gbps
・4.9152 Gbps
・2.4576 Gbps
1)
I believe DS250DF230 doesn't support 2.4576 Gbps data rate.
Is my understanding correct?
2)
Is it possible to use calibration clock both 25MHz and 30.72MHz for data rates above?
I saw Table 25 and Table 27 in Programmer's Guide however I couldn't judge if these data rates are supported or not.
Best Regards,
Yaita