Part Number: DS90UB948-Q1
Hi.
We are using DS90UB948 with DS90UB941.
We also use Power over Coax (not differential).
We have used the TI information on POC for FPD Link III for cameras as the display circuits miss this information:
The picture is transfered without problem but the back channel/configuration channel are very disturbed. The I2C link hardly works.
Soo some questions:
1) Is the POC filter recommended for FPD-Link III camera side also valid for the display link.
2) I can not find information of the frequency range used for the back-channel. We need to understand the dimensioning of the POC filter and critical frequencies.
3) 10uH is recommended for camera side. Is this valid for the display link?
4) The deserializer have an equalizer function to adapt to long/aged cables. Does the serializer have this function for the back channel?
BR
Tomas Redelius
Stoneridge Sweden