Part Number: SN65DSI86
Hi team
Need some help with this, here is the customers question, this is a USBC application
We are using TI’s SN65DSI86 MIPI DSI to eDP bridge IC. As I work through the physical layout of the USB superspeed pairs, I am struggling to determine the exact length matching requirements for the display port auxiliary mode. I am hoping you can help.
At the moment, I have inter-lane USB pairs matched to <5mils (TX1P/TX1N). It is my understanding that the display port mode uses TX1 and RX1 together as video output and must be synced together. I am wondering if your chip has the ability to adjust for minor propagation delay variation between TX1/RX1 and TX2/RX2. If so, how much variation can it adjust for? What is the overall length matching/delay requirement to avoid issues?
Thanks
Jeff Coletti