Part Number: DS90UB936-Q1
Hi all,
I have a question about connecting DS90UB913 and DS90UB936-Q1.
Input signal to GPIO of UB936. No signal is output from GPIO of UB913.
Do you know the reason for not outputting?
The register setting of UB913 is 0x0D = 55h (default).
The register setting of UB936 is 0x0F = 7Fh (default), 0x11 = 00h (default).
I have something to caring about.
UB913 has 4 GPIOs. UB936 has 6 GPIOs.
I think the number of input and output GPIOs is different.
Please give me some advice.
Best Regards,
Ishiwata