Part Number: TCA9545A
Dear Bobby
I’m inoue.
Thank you for answer the "TCA9545A: VCC rising time".
I have additional three questions.
>a bad PoR causing the state machine of the device to start up in an unknown state
1)If the device starts up in an unknown state,
Is the state fixed after sending the first Read or Write command?
>Toggling the SCL pin 8 times should resolve the issue but is not a 100% guarantee.
2)What are the concerns that are not 100%?
3)What should be the SDA state when the SCL is toggled 8 times? Don’t care?
Inoue