Part Number: TCA9803
Other Parts Discussed in Thread: TCA9517A
Hello guys,
One of my customers is consideitng using TCA9803 for their next products.
They want to get any answer to the following questions. Could you please tell me your answers to the questions?
Q1, Which VCC side (side A or side B) should be connected to I2C master device?
If the master device I/O ports working voltage is 2.5V, slave device working voltage is 3.3V, should the master device be connected to VCCA side because VCCA operation voltage range (0.8V~3.6V)
is lower than VCCB one?
Q2. What factors or conditions determine which power side to connect to the master device?
Q3. What are main different points between TCA9803 and TCA9517A? Are those working voltage range and internal pull-up current source on side-B?
Your reply would be much appreciated.
Best regards,
Kazuya.