Part Number: XIO2001
Hi, when I have this device connected to the host computer it gets stuck during boot up and the operating system will not load. I am following the power up sequence for the XIO2001. When I power on the XIO2001 after the host computer has booted up I am able to see the device using the Windriver tool and the RW-Everything tool, and get back the correct Device ID, Vendor ID, and Class Code. I tried installing the drivers for it with the Windriver tool but that caused the host computer crash and then getting stuck during boot up again.