This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822IF: Link Time

Part Number: DP83822IF

Hi,

Please tell me the following.The setting is 100BASE-FX and Signal Detect is conected and used.

We received a response that the link time from reset release should be< 1s.when the power is already ON and reset is applied.

We use the fixed mode instead of the auto negotiation.

Please tell me the reason why  the  link time is < 1s.  

Is htere any condition to shorten  the  link time?

Regards

  • Hello,

    That number was just an estimate, this is not a specification on the datasheet. The best way to estimate link time would be to measure it. The link time will also depend whether you are using the PHY in force mode or auto-negotiation.

    Thanks,

    Vibhu