Part Number: DP83867E
Hello,
I will be using TI DP83867E PHY chip on my designs. I have couple questions:
1-) INT / PWDN, I would like to pull down this pin to power down the component(has already an internal pull-up 9k so I need a stronger pull down) when my board wakes up and let my FPGA/Processor to decide to enable it. On the other hand, I also want to use the interrupt pin. But TI recommends an external 2.2k pull-up resistor for interrupt pin. Is there anyway that I can use both functionalities? This 2.2k pull up resistor is mandatory?
2-) TI recommends not to leave input pins float, If we leave I/O pins float, would it be a problem? For example, LED_1 pin? Do I also need to pull this pin down?
Best Regards,
Onur