This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN4550-Q1: CAN WUP be Disabled by Register

Part Number: TCAN4550-Q1
Other Parts Discussed in Thread: TCAN4550

Hi, 

Customer would like to disable the WUP function, could we set INH_DIS=1 and nWKRQ_CONFIG=0 to disable the WUP function for the system? Thanks. 

  • Wayne,

    This will lower the current consumption is standby mode, but the device will still transition from sleep to standby if a WUP event occurs, This function can't be disabled, however, externally your system won't technically know through any indication from the TCAN4550. Though SPI will be re-enabled in standby mode.

    Regards,