Part Number: TPS65987D
Other Parts Discussed in Thread: BQ25703A
Hello,
I have a couple of questions regarding the use of the TPS65987D in a system without SPI flash where the PD controller acts as an I2C slave to a host MCU:
- What is the absolute minimum amount of flash on the host MCU that must be allocated for the TPS65987D patch file?
- Can any of the devices registers/configurations be changed dynamically i.e. without requiring a POR and rewriting of the entire patch file?
- Does the entirety of the patch have to be written at power-up or is it possible for this to be burned into the devices ROM via the host MCU?
Thanks!
Chris