This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DPHY440SS: temperature and schematic

Part Number: SN65DPHY440SS

Hi team,

My customer have problem when using the SN65DPHY440SS. They find that the picture is flicker when the ambient temperature is 50 degree.

The following is the connection

If A is 30cm, it's works well. But if A is 70cm , the picture is flicker in 50 degree. the following is the schematic. Could you please help review it? Thanks!

Best regards

Ella