Part Number: TCA9617A
1. Could VCCA powered earlier than VCCB?
2. If VCCB and EN are powered, but VCCA kept not powered, will this device works well or have a potential risk?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9617A
1. Could VCCA powered earlier than VCCB?
2. If VCCB and EN are powered, but VCCA kept not powered, will this device works well or have a potential risk?
Hey Anders,
Anders Yang said:Part Number: TCA9617A
1. Could VCCA powered earlier than VCCB?
[Bobby] Section 10 of the power supply requirements states this is not allowed. The B version of this device does allow for A side to be larger than B side without any issues occuring.
2. If VCCB and EN are powered, but VCCA kept not powered, will this device works well or have a potential risk?
[Bobby] VccB should power up before VccA so in this case, there should be no problem.
Thanks,
-Bobby
Hi, Bobby
For the question 2, when VCCB and EN are powered, but VCCA is not powered, I want to know if the VCCB side SDAB/SCLB are tied to GND or some undetermin state by VCCA side SDAA/SCLA? Becasue VCCA is not powered.
Thanks.
Hey Rudong,
"For the question 2, when VCCB and EN are powered, but VCCA is not powered, I want to know if the VCCB side SDAB/SCLB are tied to GND or some undetermin state by VCCA side SDAA/SCLA? Becasue VCCA is not powered."
No, the device is held in 'reset' mode until VccA powers up so the device will be high impedance until then.
The only problem A version of this device has is if A side sees power before B side. If B side powers up before A side, the device will work as intended (even if A side has no power).
-Bobby
Hi, Bobby
thanks for your feedback.
one more question, when when VCCB and EN are powered, but VCCA is not powered, both SDAB/SCLB and SDAA/SCLA are in high impedance state, right?
or just SDAA/SCLA is in high imedeance state?
thanks.
rudong shi said:Hi, Bobby
thanks for your feedback.
one more question, when when VCCB and EN are powered, but VCCA is not powered, both SDAB/SCLB and SDAA/SCLA are in high impedance state, right?
[Bobby] Correct because in this situation the device is in reset.
or just SDAA/SCLA is in high imedeance state?
[Bobby] The TCA9617A is in reset and disabled while VccB and ENable is up but VccA is down.
thanks.