Part Number: XIO3130
Hello,
I am using XIO3130 in my current design and below is the configuration to be used for the same.
- There are Two XIO3130 used in Design so there are total 6 Antennas (3 Antenna per XIO3130).
Results:-
- At Power On the Board, All 6 Antennas are detected in u boot without connected the Antenna Boards.
- After connected the Individual Antenna Board on Antenna connectors, It will detect the Antenna in U boot for Individual Antenna..
- After connected the First Three(1,2 & 3) Antennas and kept rest Three (4,5 & 6) open, It will detect the First Three Antennas.
- After connected the Second Three(4,5 & 6) Antennas and kept rest Three (1,2 & 3) open, Behavior is random for second Three Antennas,
- sometime It will detect 1 or 2 Antenna
- sometime it will not detect any Antenna
- When I connect all Six Antennas simultaneously, It also have the random result, as mentioned below,
- First three Antennas will detect and rest three will not detect.
- Port for Antenna 4,5 & 6 will not shown in u boot.
- Only Four Antennas (1,2,3 and any one from 4,5,6) will shown in u boot
Requirement:-
After connecting all six Antennas in Antenna Connector, It will detect all six Antenna Boards at same time.
Is there any timing need to match to operate two XIO3130 simultaneously ?
Regards,
Alpesh