This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IO-EXPANDER-EVM: TCA6416A IC,incompatible with the GUI installer

Part Number: IO-EXPANDER-EVM
Other Parts Discussed in Thread: MSP430FR6989, TCA6416A

Hi Bobby,

I have the same issue as Blesson. I have populated the IO Expander EVM with the TCA6416A IC. The eval board is connected to the launchpad MSP-EXP430G2ET. When I try to flash the MSP430, it gives the error "Could not find device (or device not supported))". From your reply, I understand that the MSP430  I am using may be incompatible with the GUI installer since the GUI was meant to interface with version 1.5 of the MSP430G2. You suggest to set up the MSP430 to send I2C commands directly to the EVM through the SDA/SCL pins. Could you provide a detail steps for it? 

Thanks

Best Regards

Xiaolan