Part Number: SN65DSI83
Other Parts Discussed in Thread: DS90UB941AS-Q1
Hi ,
We are using SN65DSI83ZQER in our application with iMx8mini but Logic high and logic low DC analysis shows that it is not compatible with the processor. I have shared the data for your reference.
| Logic High | ||||||
| S.No | Driver | VOH(min) (V) | IOH (mA) | Receiver | VIH(min)(V) | IIH(uA) |
| 1 | IMX8M Mini | 1.44 | (1.6/3.2/6.4/9.6) | SN65DSI83ZQER | 1.26 | 0 |
| 2 | SN65DSI83ZQER | 1.25 | 4 | IMX8M Mini | 1.26 | 30 |
| Logic Low | ||||||
| S.No | Driver | VOL(max) (V) | IOL (mA) | Receiver | VIL(max)(V) | IIL (uA) |
| 1 | IMX8M Mini | 0.36 | (1.6/3.2/6.4/9.6) | SN65DSI83ZQER | 0.54 | 0 |
| 2 | SN65DSI83ZQER | 0.4 | 4 | IMX8M Mini | 0.54 | 30 |
Can you suggest any alternate of SN65DSI83ZQER which is compatible or validated with iMx8mini ?
| SN65DSI83ZQER |