This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD06: Can I connect A pin of one SN65HVD06 to B pin of another SN65HVD06?

Part Number: SN65HVD06
Other Parts Discussed in Thread: THVD1505

Hi Expert,

I am using SN65HVD06, I want to confirm if I can cross connect the RS485 bus pin(A and B pin of SN65HVD06)?

For example, there are two SN65HVD06 devices in my system, can I connect A pin of one SN65HVD06 to B pin of another SN65HVD06? See below connection.

Thank you!

Rachel

  • Hi Rachel,

    Electrically it is fine to connect the devices in this way. The Maximum differential output voltage for SN65HVD06's driver is Vcc and the receiver can tolerate +-12V differentials. However, the data on the R pins would be inverted in this configuration and may need to be corrected for with other circuitry or programming. Similarly, the crossed transceiver will drive an inverted signal onto the bus. 

    You may consider a device which features polarity correction for this application such as THVD1505. This device is typically used for hot-insertion applications to correct for swapped A-B inputs and may also be useful in your application. 

    Let me know if you have any more questions about SN65HVD06 or THVD1505 in your application. 

    Regards,

    Eric

  • Hi Eric,

    Thanks for your reply, this resolved my question

    BR 

    Rachel