Part Number: DP83825EVM
Other Parts Discussed in Thread: MSP430F5529, USB-2-MDIO
Hello Team,
I am trying to flash MSP430F5529 following USB-2-MDIO Software Tool user guide 2.3.1 Flashing MSP430G2 LaunchPad and encounter problem flashing the F5 launchpad. After clicking on F5.bat file, the message shows error in driver. I would like to clarify if there is a hardware problem.
In 2.2 Hardware Setup MSP430F5 Series, it says "To properly configure the F5 Series, the user will need to remove the 3V3 jumper located between the 5V and RTS jumpers.Connect the desired I/O voltage to the 3V3 header located at J10." Is it required to supply a external 3.3V to J10 on F5 launchpad when flahshing F5 launchpad?
Thank you.
Regards,
Ting