Part Number: DS90UB941AS-Q1
Hello,
We are developping a product using the 941 / 948 SerDes configuration
The first version worked fine with the chip revision :
- GPIO_0_Config (0x0D) REV_ID = 0010
The new revision is using a new SoC, and we only see half of the screen, even when are displaying the pattern of the IC (color bar ...)
- GPIO_0_Config (0x0D) REV_ID = 0011
When we change the DSI config of the SOC we see no change on the screen.
Both are using the exact same screen, and reads TX_ID (0xF0 to 0xF5) = _UB941
The Pixel data rate is 71MHz, the resolution is 1280 x 800 x 60
We use 1 FPD Link lane in coax.
The configuration is :
MODE0 = 4
Split = 0
DSI Lane =4
MODE1 = 3
Clock = 0
Coax = 1
Disable DSI = 0
IDx = 0x0C
Is there a specific register which could explain this behaviour ? or if there is a difference between both IC revision ?
Thanks,
Best regards,
Alexandre