Part Number: TCAN1042HGV
One TCAN1042HGV is connected to the CAN bus. When a second TCAN1042HGV is connected to the CAN bus, it drags down CAN HI and CAN LO during it’s power up sequence..
In this implementation during power up the VCC (5V converter) comes up first, then 200ms later the VIO (3.3V converter) powers on. After the 3.3V VIO converter is running, the CAN bus returns to normal.
Are there any sequencing requirements for VCC and VIO on this part? The data sheet seems to contains no information about this topic?