Part Number: DS90UB954-Q1
Dear TI,
We were using the 954 Deser in our design together with external 25MHz clock without problem, in Synchronous mode, since we had EMC problems we tried to use clock with Spread Spectrum feature, we are using in this case the same clock, but this clock has a PIN which you can use to enable or disable the Spread Spectrum, now we have a problem, because the connection 954/953(We have two 953 connected by POC) is not working, only when we enable the SS feature in the clock. Sometimes works, but the most time is not working, looks like timing problem, but I would like to ask you, about if the specs of our clock with Spread Spectrum are full filing the 954 specs, I think so but...
These are our Clock Specs...
Thanks and best regards