Part Number: TSB41BA3B-EP
Hi all:
I use TSB41BA3B-EP to design a 1394 distributor, that is, the 1394 signal source sends data to port0, and port1 and port2 are connected to two devices to receive the data from the signal source. During the test, it was found that the signal source and my splitter could not establish a connection: The check found that the interval of the tone signal output from the TPB port of the 1394 signal source was about 42ms, as shown in Figure 1, but the interval of the tone signal output from the TPB port of the 1394 distributor port0 127.7ms, as shown in Figure 2.
Could the connection not be caused by this problem? Or other problems.
Very anxious, thank you.Attached is my schematic.
fig 1
fig 2