Part Number: DS15BR400
For unused inputs like IN2+/- (pins 13/14) and IN3+/- (pins 15/16). Can those be left unconnected if not used?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS15BR400
For unused inputs like IN2+/- (pins 13/14) and IN3+/- (pins 15/16). Can those be left unconnected if not used?
Hi Lindsey,
The unused inputs should be tied off as listed below to ensure the outputs remain in a stable state.
IN+ = 3.3K to VDD
IN- = 3.3K to GND
This will ensure 50mV of offset at the input which is enough to keep the output from switching.
Regards,
Lee