This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IR: Link fails

Part Number: DP83867IR


Hi all.

I've been working with this part on a custom board, and suddenly the port does not link up to my host.  I tested the host port.  It's fine.

The configuration hasn't changed.  Measuring the 4 RJ-45 pairs with the ieee test #1 mode shows that three of the 4 pairs look correct as far as the ieee test #1 waveform, but the waveform on the 4th line has an amplitude that is way too high.  The peak voltage on the square wave part. are about 1.5 volts, and the pulses are over 1 volt.  The terminator on the wild pair is good. 

It appears to me that the PHY is faulty, but I would like to hear from someone with more experience with this part.  Any other ideas?