Other Parts Discussed in Thread: TRS3122E
Hi team,
Can PCA9306 be used for RS232 UART TX RX 115200 bps level translation? 1.8V to 3.3V?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Jack,
Yes, this device could be used to translate UART communication between those two voltage levels. Just be sure to follow the recommended connections in the datasheet (including pull-up resistors on the SDA/SCL IOs on both sides, which may not be required by the UART but would be required by PCA9306).
If you actually needed RS-232 voltage levels (i.e., to interface to an external RS-232 port), you could connect the 1.8-V or 3.3-V logic lines to an RS-232 transceiver. Please let us know if you need help selecting a transceiver device. For example, TRS3122E might be something to consider since it is able to interface to either 3.3-V or 1.8-V UART signals.
Regards,
Max
Hi Jack,
I can see how PCA9306 could be suited for this application. There doesn't seem to be any glaring problems, but in any use-case apart from intended, I would advice some careful considerations:
I will keep you notified if I become aware of other important considerations. Let me know if you have any other questions.
Regards,
Eric