Part Number: TPS65987D
Other Parts Discussed in Thread: BQ25703, BQ4050, , TPS65981
Hello,
I have a customer who is using the TIDA01515 as a baseline for their design. They are suing the TPS65987D instead but still using the BQ4050 and BQ25703.
They've got the BQ4050 working and communicating with the TPS65987DDHRSHR using the 'TPS65981_2_6_7_8 Application Customization 5.13' tool (both through I2C debug and programming the Flash through SPI).
So far they've just been using the standard settings built into the 'TPS65981_2_6_7_8 Application Customization 5.13' tool for TPS65987DDH.
They don't see any activity (ie the transistors aren't turning ON) on the BQ25703ARSN and they are wondering if the settings in the 'TPS65981_2_6_7_8 Application Customization 5.13' tool include features to talk to the BQ25703ARSN?
They don't see settings in there regarding the BQ25703ARSN so it makes me wonder if I need a special setup to allow the TPS65987DDHRSHR to control the BQ25703ARSN?
I don't see any software for the TIDA-01515 to address this.
Thanks,
Nick