Part Number: DS90LV047A
Other Parts Discussed in Thread: DS90LV048A,
Hello, experts,
I have inquiries about DS90LV047A / DS90LV048A.
Each datasheets describe "The DS90LV048A is a quad receiver device, and if an application requires only 1,2, or 3 receivers, the unused channel(s) inputs must be left OPEN." at 8.3.1 LVDS Fail-Safe.
How about the case of the DS90LV047A unused channel(s) inputs/outputs?
Are there any problem when the driver/receiver unused channels inputs/outputs are left to connect to Vcc(=3.3V)?
The reason of asking is that the customer who use these ICs is planning to replace ROHM IC with TI IC as P2P, and ROHM IC is recommended to be connected to Vcc.
I have seen
https://e2e.ti.com/support/interface/f/138/t/502244
https://e2e.ti.com/support/interface/f/138/t/736989
, but I don't understand well.
Best regards,
Hideki