Other Parts Discussed in Thread: TUSB320, TPS25910
Hello,
I am trying to use the evaluation module to apply power to a phone while a microcontroller is attached in USB OTG mode.
The goal is to charge the phone while it is in USB OTG and the microcontroller is attached via USB2.0 and the microcontroller will provide power to the phone. The controller has it's own large battery to keep the phone topped off. I have a Cypress Semiconductor EZ-PD that is able to charge while in USB OTG, but I want to stay with all TI brand chips in this product.
I am able to get USB communication or charging, but not both same time. I have pin 1 on, and tried all variations of pin 7-8 for different modes. I shorted the diode for D9 and D11. I can only get charging mode if manually jumper the ID pin to GND on J2.