Part Number: LMH1218
Hello community,
We have an application using either IN0 or IN1 of LMH1218 to fanout both on OUT0 and OUT1. We need OUT1 output clock divided by 40 (0x1C: OUT1 puts out line rate clock for 3G and below and 297 MHz clock for 5.94Gbps and 11.88Gbps) and at the same time OUT0 output the re-timed data.
Thus, there are two application scenarios:
1) using IN0 as data input, OUT1 output a clock and OUT0 output the re-timed data;
2) using IN1 as data input, OUT1 output a clock and OUT0 output the re-timed data.
Is this available?