Part Number: TUSB3410
Other Parts Discussed in Thread: TUSB9261
Hi SIr,
Could TUSB3410 support USB to SPI convert or not?
If not, do we have other solution could achieve USB to SPI convert?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Update
I see the TUSB9261 have two SPI port, will this support USB to SPI convert?
But this one is overkill, do we have an easy solution for this?
The application is as below,
Want to use SPI to communicate with CPLD, but CPU don't have SPI, only USB, so we want to use USB to SPI convert to achieve this.
Thank you.
Hi Penn,
Unfortunately, TUSB3410 and TUSB9261 can not support this application. TUSB9261 is only USB to SATA and TUSB3410 does not have SPI capability only I2C. TUSB9261 only has 1 SPI interface for EEPROM loading, extra SPI Chip Select pins are not full SPI interfaces.