Part Number: TPD6S300
Other Parts Discussed in Thread: , STRIKE
What's the difference between TPD6S300A and TPD6S300? Which should I promote to customer?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The largest difference is that the TPD6S300A keeps the USB Type-C port connected during an IEC 61000-4-2 ESD strike. The TPD6S300A also has improved dead battery performance. Check out section 8.3.5 in the TPD6S300A datasheet for more information on each of these improvements. If the customer is looking for a protection device that keeps the USB Type-C port connected during an ESD strike or needs the dead battery improvements that accompany the TPD6S300A, please recommend the TPD6S300A.
Thanks,
Emma