Part Number: DS90UH949-Q1
Hi
Now i am doing testing using DS90UH949-Q1 + DS90UB940 EVM.
May i ask how to disable DS90UH949-Q1 HDCP so it can work with DS90UB940 ? thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UH949-Q1
Hi
Now i am doing testing using DS90UH949-Q1 + DS90UB940 EVM.
May i ask how to disable DS90UH949-Q1 HDCP so it can work with DS90UB940 ? thanks!
Hello PYTsai,
HDCP is not active by default on 949 but if for some reason you have activated it and need to disable it, then set bits 0xC3[3] and 0xC3[1] = 1 on the 949
Best Regards,
Casey
Hi Casey,
The attachment is our DS90UH949-Q1 register dump. How to read it to check if the HDCP of DS90UH949-Q1 is on or off ?
[REGISTERS] Device = ALP Nano 1 - DS90UH949, Connector 1 Comments = "DS90UH949 Register dump" Date = 01/16/2020 Time = 13:32:28 Reg = 0,0x0000,0x18 Reg = 0,0x0001,0x00 Reg = 0,0x0003,0xDA Reg = 0,0x0004,0x80 Reg = 0,0x0005,0x00 Reg = 0,0x0006,0x58 Reg = 0,0x0007,0xA0 Reg = 0,0x0008,0xB0 Reg = 0,0x0009,0x00 Reg = 0,0x000A,0x00 Reg = 0,0x000B,0x00 Reg = 0,0x000C,0x01 Reg = 0,0x000D,0x10 Reg = 0,0x000E,0x00 Reg = 0,0x000F,0x00 Reg = 0,0x0010,0x00 Reg = 0,0x0011,0x00 Reg = 0,0x0012,0x00 Reg = 0,0x0013,0x88 Reg = 0,0x0014,0x00 Reg = 0,0x0015,0x01 Reg = 0,0x0016,0xFE Reg = 0,0x0017,0x1E Reg = 0,0x0018,0x7F Reg = 0,0x0019,0x7F Reg = 0,0x001A,0x01 Reg = 0,0x001B,0x00 Reg = 0,0x001C,0x00 Reg = 0,0x001D,0x00 Reg = 0,0x001E,0x05 Reg = 0,0x001F,0xF5 Reg = 0,0x0020,0x0B Reg = 0,0x0021,0x00 Reg = 0,0x0022,0x25 Reg = 0,0x0023,0x00 Reg = 0,0x0024,0x00 Reg = 0,0x0025,0x00 Reg = 0,0x0026,0x00 Reg = 0,0x0027,0x00 Reg = 0,0x0028,0x01 Reg = 0,0x0029,0x20 Reg = 0,0x002A,0x20 Reg = 0,0x002B,0x80 Reg = 0,0x002C,0x00 Reg = 0,0x0030,0x00 Reg = 0,0x0031,0x00 Reg = 0,0x0032,0x00 Reg = 0,0x0033,0x00 Reg = 0,0x0034,0x00 Reg = 0,0x0035,0x00 Reg = 0,0x0036,0x00 Reg = 0,0x0037,0x00 Reg = 0,0x0038,0x00 Reg = 0,0x0039,0x00 Reg = 0,0x003A,0x00 Reg = 0,0x003B,0x00 Reg = 0,0x003C,0x00 Reg = 0,0x003D,0x00 Reg = 0,0x003E,0x00 Reg = 0,0x003F,0x00 Reg = 0,0x0040,0x14 Reg = 0,0x0041,0x4E Reg = 0,0x0042,0x00 Reg = 0,0x0043,0x00 Reg = 0,0x0044,0x80 Reg = 0,0x0045,0x00 Reg = 0,0x0046,0x00 Reg = 0,0x0047,0x00 Reg = 0,0x0048,0x01 Reg = 0,0x0049,0x68 Reg = 0,0x004A,0x01 Reg = 0,0x004B,0x00 Reg = 0,0x004C,0x00 Reg = 0,0x004D,0x00 Reg = 0,0x004E,0x00 Reg = 0,0x004F,0x00 Reg = 0,0x0050,0x17 Reg = 0,0x0051,0xA1 Reg = 0,0x0052,0x1E Reg = 0,0x0053,0x00 Reg = 0,0x0054,0x28 Reg = 0,0x0055,0x0C Reg = 0,0x0056,0x00 Reg = 0,0x0057,0x00 Reg = 0,0x0058,0x00 Reg = 0,0x0059,0x00 Reg = 0,0x005A,0x92 Reg = 0,0x005B,0x20 Reg = 0,0x005C,0x02 Reg = 0,0x005D,0x06 Reg = 0,0x005E,0x44 Reg = 0,0x005F,0x00 Reg = 0,0x0060,0x22 Reg = 0,0x0061,0x02 Reg = 0,0x0062,0x00 Reg = 0,0x0064,0x10 Reg = 0,0x0065,0x00 Reg = 0,0x0066,0x00 Reg = 0,0x0067,0x00 Reg = 0,0x0068,0x00 Reg = 0,0x0069,0x00 Reg = 0,0x006A,0x00 Reg = 0,0x006B,0x00 Reg = 0,0x006C,0x00 Reg = 0,0x0070,0x00 Reg = 0,0x0071,0x00 Reg = 0,0x0072,0x00 Reg = 0,0x0073,0x00 Reg = 0,0x0074,0x00 Reg = 0,0x0075,0x00 Reg = 0,0x0076,0x00 Reg = 0,0x0077,0x00 Reg = 0,0x0078,0x00 Reg = 0,0x0079,0x00 Reg = 0,0x007A,0x00 Reg = 0,0x007B,0x00 Reg = 0,0x007C,0x00 Reg = 0,0x007D,0x00 Reg = 0,0x0080,0x00 Reg = 0,0x0081,0x00 Reg = 0,0x0082,0x00 Reg = 0,0x0083,0x00 Reg = 0,0x0084,0x00 Reg = 0,0x0090,0xA7 Reg = 0,0x0091,0x4C Reg = 0,0x0092,0x31 Reg = 0,0x0093,0xBD Reg = 0,0x0094,0xA8 Reg = 0,0x0098,0x00 Reg = 0,0x0099,0x00 Reg = 0,0x009A,0x00 Reg = 0,0x009B,0x00 Reg = 0,0x009C,0x00 Reg = 0,0x009D,0x00 Reg = 0,0x009E,0x00 Reg = 0,0x009F,0x00 Reg = 0,0x00A0,0x00 Reg = 0,0x00A1,0x00 Reg = 0,0x00A2,0x00 Reg = 0,0x00A3,0x00 Reg = 0,0x00C0,0x05 Reg = 0,0x00C1,0x00 Reg = 0,0x00C2,0xC0 Reg = 0,0x00C3,0x00 Reg = 0,0x00C4,0x28 Reg = 0,0x00C5,0x00 Reg = 0,0x00C6,0x00 Reg = 0,0x00C7,0x60 Reg = 0,0x00C8,0xC0 Reg = 0,0x00C9,0x00 Reg = 0,0x00CA,0x00 Reg = 0,0x00CB,0x00 Reg = 0,0x00CC,0x00 Reg = 0,0x00CE,0xFF Reg = 0,0x00D0,0x10 Reg = 0,0x00D1,0x00 Reg = 0,0x00D2,0x00 Reg = 0,0x00D3,0x00 Reg = 0,0x00E0,0x05 Reg = 0,0x00E1,0x00 Reg = 0,0x00E2,0xC0 Reg = 0,0x00E3,0x00 Reg = 0,0x00E4,0x28 Reg = 0,0x00E5,0x38 Reg = 0,0x00E6,0x00 Reg = 0,0x00E7,0x00 Reg = 0,0x00F0,0x5F Reg = 0,0x00F1,0x55 Reg = 0,0x00F2,0x48 Reg = 0,0x00F3,0x39 Reg = 0,0x00F4,0x34 Reg = 0,0x00F5,0x39 Reg = 0,0x00F6,0x00 Reg = 0,0x00F8,0x00 Reg = 0,0x00F9,0x00
Hello PYTsai,
According to the register dump, 0xC4[0] = 0 which means HDCP is not authenticated. Also 0xC3 = 0x00 which shows encryption is not enabled.
Best Regards,
Casey