Part Number: DS90UB964-Q1
Hi TI Experts,
We have DS90UB964-Q1 Desrializer on our MIPI CSI2 solution boards connected to the processor.
I like to know if DS90UB964-Q1 can generate test pattern for below
1. RGB565 color bar with 4096x4096 resolution
2. RAW8 color bar with 4096x4096 resolution
From the Data sheet I could infer the default Dat type 0x24 (RGB888).
Can I change this to 0x22 (RGB565) or 0x2A (RAW8) and generate the desired color bar patterns?
If DS90UB964-Q1 Desrializer does not support these formats, then please let me know which other Deserializer can be used.
Thanks,
Sathyakam